Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
open-loop-slide11

Open loop hall effect current sensor specifications define the input current as the rated, primary, or, nominal current rating of the current sensor as a DC or RMS current. The output voltage of the open loop current sensor is an instantaneous output voltage representation of the primary current whether DC or AC. Therefore, the output voltage tracks the input current exactly; there is no RMS conversion made by the current sensor.

PTM פורסם ב: