Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide11

The plot on this slide illustrates the high efficiency of the 48V output GWS250, peaking at 93% at 230VAC input. The average efficiency is calculated by using measurements made at 25, 50, 75 and 100% load and this result is achieved by having a flat efficiency characteristic, which is important as most users do not operate the power supply at full load.

PTM פורסם ב: