Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide6

A standby voltage is also provided as a standard feature. This output is rated at 5V, 0.3A, and has a voltage regulation of 4.75V to 5.25V. This voltage is present as long as AC power is applied to the GWS, even when the remote ON/OFF is utilized. The 24V and 36V models have a peak power rating of 300W. This peak power can be drawn for up to ten seconds on a 35% maximum duty cycle. Care should be taken to ensure that the average power drawn does not exceed 250W.

PTM פורסם ב: