Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
GWS250-Slide5

Using the voltage program feature, the output voltage of the GWS250 can be adjusted over a wide range, as shown on this slide. The bottom right hand graph shows the external voltage level required to program the output. For example, to set the output voltage of the GWS250-24 to 28.8V, apply 6V to the "PV" terminal.

PTM פורסם ב: