Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
HiDef-Slide22

The HDO4000 series delivers bandwidths of 200MHz and 350MHz in two-channel versions, and bandwidths of 200MHz, 350MHz, and 500MHz and 1GHz in four-channel versions. Maximum sampling rate on all channels is 2.5 GS/s. There is 12.5 Mpts/ch of memory and a maximum of 50 Mpts. The mixed signal versions add 16 digital channels with a digital sampling rate of 1.25 GS/s. Minimum detectable pulse width is 2ns and maximum input frequency is 250MHz.

PTM פורסם ב: