Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Capacitive Touch Sensing Slide 15

Duty cycle is a key component to power consumption. A large duty cycle will result in a slower response time, and therefore decreasing power consumption. As shown here, if the user were to sample at 2 Hz, the average power consumption would be ~1.3 µA. For 99% of the measurement time, the device is in low power mode allowing the CPU to be used for other tasks.

PTM פורסם ב: