Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
Capacitive Touch Sensing Slide 11

In this demonstration the TI_CAPT_Custom function is used. The Custom function incorporates a baseline tracking feature. This feature allows the algorithm to compensate or track slow capacitance changes caused by the environment and prevents these changes from triggering false detections. The graph is showing the delta between the baseline and the measured value. This delta is used to determine the appropriate threshold levels for the application.

PTM פורסם ב: