Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
NFC Link Part 2 Slide 11

The same Tag Type 4B (RF430CL330H), which has been formatted with the tool and then programmed with an image (MIME). This demonstrates a larger file being stored, which could then be extracted out of the tag by another NFC device or via the host over I2C or SPI.

PTM פורסם ב: