Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
NFC Link Part 2 Slide 20

The user can also set up two of the hardware sets and run two instances of the GUI on the same PC (with one as reader/writer and the other in card emulation mode) then read/write data without using an NFC handset. Shown here is an example of writing a ~5.7 kB image and reading it back.

PTM פורסם ב: