Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
NFC Link Part 2 Slide 6

The user can now enter data into the bottom ‘Write’ window and press the Write button to write NDEF message into the tag. When this occurs, the screen will quickly flip to Write NDEF, then the user can either press the Read button or remove the tag from the reader/writer antenna and re-present the tag to get the NDEF message read back. The NDEF size is now 236 bytes (out of 250 bytes available on the tag) and the message is displayed.

PTM פורסם ב: