Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
TMC2100 Slide 12

In a minimum setup, the RC-Filter for VCC can be eliminated. Further, the sense resistors can be eliminated by replacing them with a single reference resistor (Rref). The peak coil current is adjusted by Rref to 3000 times the current flowing into AIN_IREF pin (calculate with about 4.8 V at Rref). To use this option, leave pin CFG3 floating.

PTM פורסם ב: