Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Product List
TMC2100 Slide 4

The TMC2100 can be driven by any step and direction source. As no configuration is required, a minimum of two control wires is sufficient. An optional feedback provides index position pulses as well as driver error information. Additionally, an optional analog voltage generated by a DAC or by microcontroller PWM plus R/C filter can be used for motor current control.

PTM פורסם ב: