Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Common Mode Chokes Slide 6

There are two ways to wind the core for a common mode choke. The first is using sectional windings. This is made up of two independent windings wound separate of each other. The second would be the Bifilar way of winding which incorporates two wires wound around the core together. As will be shown in the next couple of slides, bifilar windings do not improve differential mode impedance whereas Sectional windings will. Würth supplies common modes with both types of windings.

PTM פורסם ב: