Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
Common Mode Chokes Slide 8

By adding the sectional winding to the circuit, the differential mode impedance increases to the point where, at 1MHz, there is over 10 Ω of impedance attenuating the lower frequency spectrum. This increase is due to the leakage inductance that is induced between the separate windings. This acts in series with the load to provide differential noise filtering.

PTM פורסם ב: