Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide14

Referring to the two plots shown on this slide, the green trace is the current as measured in the short circuit. The fault is latched if the device remains clamped for at least 1µs. This clamp time is provided to allow current to charge the varistor present in most brushed DC motors. Overcurrent is not intended to limit inrush current.

PTM פורסם ב: