Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide19

Initially the driver implements fast decay with synchronous rectification. This is effectively a direction change and results in a short of the BEMF voltage in the load, resulting in rapid current decay. After 50% of the off-time, the device enters slow decay. When the current regulation is close to zero, there is load reversal protection which prevents the current from changing polarity during fast decay by sensing the current level and automatically switching to slow decay. This results in discontinuous load current, but prevents potential reversal of the motor.

PTM פורסם ב: