Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide16

In the display on this slide, a couple periods of the PWM current control are shown. Channel 1 is the voltage at output A and channel 2 is the voltage at output B, the output current is shown on channel 4. The flow of current is from output A to output B. The PWM current controller operates in 50% mixed decay.

PTM פורסם ב: