Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
A495x-Slide3

The core family includes three drivers with a 2A peak output current rating. The A4952 and A4953 are both single full bridge drivers while the A4954 is a dual full bridge driver capable of supporting 2A per bridge. Rounding out the family is the A4950 which is a higher current version of the A4953 rated at 3.5A peak current.

PTM פורסם ב: