Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide18

What can be done to solve the RFI problem? If the interference is primarily coming through the input leads, one solution that works very well is to use a filter before the instrumentation amplifier. This filter removes the radio waves before they reach the instrumentation amplifier. It is imperative that the filtering be placed before the instrumentation amplifier before the high frequency energy can be rectified, rather than after the In Amp, where the filter will be ineffective against the already rectified (low frequency) signal. Another way to reduce RFI interference is to twist the leads connected to the instrumentation amplifier. This will reduce their ability to pick up the high frequencies and deliver them to the In Amp. If the radio interference is particularly strong, it may come in through other pins on the instrumentation amplifier or through the package itself. If this is the case, there is little that can be done other than completely shielding the circuitry.

PTM פורסם ב: