Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide2

Occasionally an application requires an instrumentation amplifier to measure a floating source. Examples of floating sources are a battery powered voltage source, a source coupled through a transformer or capacitors, or a thermocouple. Instrumentation amplifiers are not able to measure floating sources, at least not for very long. This is because instrumentation amplifiers have bias currents that will charge up the floating source until it is outside the instrumentation amplifier’s common mode input range. In order to prevent this from happening, a high value resistor should be used to give the bias current a return path to the in amp’s power supplies. This resistor is tied to a voltage source within the In Amp’s input range, typically ground. Because In Amp bias currents are normally quite small, this bias current resistor can be quite large: typically 1MΩ or more. Note that bias current resistors are not required when both the sensor and the In Amp have a return path to ground. For example if a sensor is tied to earth ground and the In Amp’s power supply is also referenced to this same earth ground, no bias current resistor is needed.

PTM פורסם ב: