Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide23

When selecting components for an RFI filter, it is important to keep a few things in mind. First, the capacitors connected to ground on each input should be well matched. NPO/C0G or X2Y capacitors are recommended. Also, the RFI filter should not be too low in frequency. The higher the RFI filter cutoff, the less effect mismatches will have on AC CMRR. The choice of cutoff is a tradeoff between the AC CMRR required and how robust the RFI rejection should be. Additionally, board layout should be symmetrical and long traces avoided. A poorly laid out board can contribute significant parasitic capacitances.

PTM פורסם ב: