Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
amplifier-performance-slide28

In summary, instrumentation amplifiers are one of the least complicated components on a typical circuit board. Because of their ease of use, the external circuitry needed for optimum performance is often overlooked. With a little thought, the full performance of the instrumentation amplifier can be realized through careful consideration of the bias current return path, driving the reference pin, input voltages near the supply rails, input voltages beyond the supply rails, potential radio frequency interference, and ensuring there are no mismatched components at inputs.

PTM פורסם ב: