Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
IPSwitches-Slide2

Simply defined, IP stands for ingress protection. IEC IP ratings traditionally have been assigned to enclosures such as circuit boxes that hold automation controls. The ratings are listed as the letters IP followed by a set of numbers that represent different levels of sealing and can range from none to “dust tight” protection and “continuous immersion in water”. The ratings were established by the International Electrotechnical Commission and can be found in IEC Publication 529.

PTM פורסם ב: