Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
IPSwitches-Slide6

Another way that IP ratings are presented are with these optional IP Code Symbols. This chart illustrates the use of symbols in the IP classification system.  Each symbol indicates a particular degree of ingress protection and many times these symbols are placed on equipment to illustrate the IP protection provided. While the wording in the table is not exactly as used in the standards document, the data accurately describes the requirement.

PTM פורסם ב: