Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PSoC 4000: Low-Cost 32-bit MCU Slide 14

PSoC 4000 supports two low-power modes: sleep and deep-sleep. The current consumption in the different modes are as shown on this slide. The PSoC 4000 family enables efficient designs with low power consumption by utilizing the deep-sleep power mode with wake-on-interrupt and I2C address detect, a watchdog timer operation, during both the sleep and the deep-sleep power modes, and an instantaneous wake-up from sleep. PSoC Creator’s API enables easy switching between the power mode and control of individual PSoC Components, enabling better power management.

PTM פורסם ב: