Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PSoC 4000: Low-Cost 32-bit MCU Slide 4

Some of the terms used in this presentation are shown on this slide. First is liquid tolerance, which is the ability of a touch-sensing solution to work properly in the presence of water droplets, streaming water, mist, or other liquids. A proximity sensor is a sensor that can detect the presence of nearby objects without any physical contact. Next is the signal-to-noise ratio or SNR. This is the ratio of the sensor signal, when touched, to the noise signal of an untouched sensor. Manual tuning is the process of configuring capacitive button parameters for optimal performance. This is required to compensate for system, manufacturing, and environmental changes.

PTM פורסם ב: