Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
usb ps2 info
Communication from the host to the microprocessor is done via USB and uses low speed USB standard, it is compatible with any USB 1.1 or 2.0 host, it enumerates as a HID device, and uses the standard Windows mouse driver. The microprocessor reports data to the host at a rate of 50 reports/second. Likewise with the PS/2 module communication from the host to the microprocessor is done via PS/2 and will attach as a standard two button mouse, or as a three button scroll mouse, it is compatible with all versions of Windows, and the microprocessor reports data to the host at a rate of 50 reports/second, regardless of host attempts to change the report rate.
PTM פורסם ב: