Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
right click
Tapping the touchpad in the upper right corner is interpreted as a “right click”. Initiating a touch on the right border edge of the touchpad will set the mouse into scrolling mode. The finger or stylus can then be moved up and down along the right edge to scroll. This feature does not activate when the border region is entered during a mouse cursor movement gesture and the border region is used for mousing only. External right, left, and center-click buttons are available via 4-pin FFC (J3) or Molex header connector (J7). Customization includes color and texture of graphic layer, multicolor graphic artwork, text and logos, orientation, and removal of features.
PTM פורסם ב: