Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
RS-Slide4

There are three common connection schemes used in interface networks. On the left is point-to-point, which can be used with either RS-422 or RS-485. Point-to-point means there is just one transmitter talking with only one receiver on a bus. A point-to-point RS-422 network is often used as an RS-232 “extension cord” to extend the transmission distance of RS-232 control lines. The multi-drop – or broadcast – network is the middle example. It has only one transmitter on the bus, but allows multiple receivers. Both RS-422 and RS-485 can operate in this configuration. RS-485 is the most flexible standard, allowing for multi-point operation, where it is possible to have multiple transmitters and receivers all on the same bus. For all schemes, a ground connection between nodes is recommended to control common mode voltage differences, and to minimize EMI.

PTM פורסם ב: