Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
RS-Slide9

The transmitter differential output comprises two identical CMOS push-pull structures on the two output pins. The NMOS output transistor in Renesas' process sources current when the output pin is taken below ground, so a diode is utilized to block the current. Adding the diode raises the low output voltage to approximately 1V, which has caused problems in some applications that tried to use RS-485 transmitters as single-ended line drivers. The PMOS device is able to function properly over the full -7V to +12V signal range, therefore no blocking diode is needed. The result is a better differential output voltage compared with transmitters that require both high- and low-side blocking diodes. Driver ESD cells are the same as those used on the receiver pins.

PTM פורסם ב: