Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
RS-Slide5

The important RS-485 transmitter output waveform is the differential signal that the receiver processes. VOD is defined as the difference between the transmitter’s non-inverting and inverting outputs, which are the Y and Z pins respectively. A common point of confusion arises from the fact that the differential waveform swings both negative and positive, causing one to think that the RS-485 transceiver must be outputting negative voltages. In reality, the negative VOD is just an artifact of its mathematical definition, and VOD is negative whenever the Z output is high and the Y output is low. The RS-485 signal’s unit interval is the same as the bit width and is the reciprocal of the data rate, and the data rate is 2x the switching frequency. Y and Z balance is very important to minimize EMI. If the Y and Z output transition times and propagation delays are well matched, then emissions from those outputs will cancel each other due to the use of twisted pair cabling.

PTM פורסם ב: