Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 10
A design engineer can have a system working with MAX31856 very quickly, there is no need to do a lot of register writing to make it work. Just enter a couple of bytes to select thermocouple type, rejection frequency, and whether the engineer wants it to convert continuously or on demand, and now the system is ready to read thermocouple temperature.
PTM פורסם ב: