Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 14
Setting up and using the MAX31856 is quick and easy, all the items required are provided in the kit from Analog Devices. Connect the K-type thermocouple to J1 of the MAX31856PMB1 with the yellow wire on the plus side. Connect the MAX31856PMB1 Pmod connector H1 to the connector on USB2PMB. Connect the USB2PMB to the PC with the Mini-USB cable. Finally, launch the MAX31856 Evaluation System GUI, it should auto detect the USB2PMB adapter or the engineer can use the Device command in the main menu to select the adapter.
PTM פורסם ב: