Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
MAX31856 Precision Thermocouple to Digital Converter with Linearization Slide 19
The challenge to the designer is that because of the small signal output and the requirement of a temperature measurement at the junction of the thermocouple and conversion circuit, complex signal conditioning with precision components is required to get thermocouple data into a language that can be read by a microcontroller. The MAX31856 from Analog Devices was introduced to solve this problem. It features internal cold-junction compensation, linearization, and data conversion, thus replacing up to six components in the discrete design. The device offers support for several thermocouple types, reducing time to market in applications that utilize multiple types.
PTM פורסם ב: