Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide12

dsPIC33 includes Direct Memory Access (DMA) controller for efficient data movement. The devices include eight DMA channels. Each of the eight channels can move data to/from eight different peripheral source or destinations. A simple arbitration scheme prioritizes each channel should more than one channel attempt transactions at the same time. The channel with the lower number wins. Note that the DMA system has its own bus for DMA transactions. This “backside” bus means that DMA transactions can occur simultaneously with CPU transactions. It is not necessary to disrupt the CPU operation or wait for a “dead cycle” in the CPU operation.

PTM פורסם ב: