Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide27

On a dsPIC33 device, with 3.3V power supply, the digital inputs nominally operate from zero to 3.3V. However, input pins that only have digital functions can sustain a 5V input. The levels at which the input pin detect a input high or input low stay the same and are set at values that work for 3.3V inputs. Input pins that have analog functions are not 5V tolerant, and cannot exceed the VDD max specification of 3.6V.

PTM פורסם ב: