Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide25

The dsPIC33 devices operate with an external supply of 3.3V ±10 percent. The internal core of the device operates at 2.5V ±10 percent. It is not necessary to provide an external regulator for the internal supply however. Because the regulator is integrated within the device, you only need to provide the 3.3V source.

PTM פורסם ב: