Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
Pt1-Slide14

Most peripheral modules are capable of interfacing to the DMA channel. The Timer 2 and Time 3 modules can initiate a DMA transaction based on a time tick. Data can be streamed from either Input capture module 1 or 2 to capture a pulse stream. Data can be streamed to either output compare module 1 or 2. This can be used, for example, to automatically stream data to a PWM, generating a tone with no CPU overhead. All of the communication peripherals are DMA enabled, allowing large message buffers to be transmitted or received with no CPU overhead. Most of the communication peripherals have a small internal buffer to allow use of the peripheral without DMA, should the data rate be manageable by the CPU. The AD modules, as a source for much of the data passing through the system, has a very flexible interface to the DMA channel, allowing data to be sorted in time or sorted by analog input.

PTM פורסם ב: