Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
mTouch-Slide10

A parallel combination of pad and finger capacitance add together to form a total sensor capacitance labeled Cs. The capacitance that is introduced by the finger is typically from 5pF to 15pF. Therefore, it is important to ensure that the pad capacitance is small so that the system acknowledges that a touch is sensed.

PTM פורסם ב: