Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
mTouch-Slide29

To accurately detect a change in frequency of the relaxation oscillator, two variables and one constant are used. The average variable keeps a running average of 16 previous samples from the TMR1 registers. This running average is used to eliminate noise created by changes in temperature, voltage, and environment. The raw variable holds the current value in TMR1 registers. The predetermined trip constant is the minimum difference between the raw data and the average value.

PTM פורסם ב: