Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
mTouch-Slide16

With regard to the SR Latch truth table, when the Set input is driven HIGH, the pin connected to the Q bar output of the latch will be driven LOW. If the Reset input is driven HIGH, the pin connected to the Q bar output will be driven HIGH. When both Set and Reset inputs are HIGH, the operation of the Latch will be in Reset mode since this Latch is Reset dominant. When both inputs are driven LOW, the outputs of the Latch will hold the last known output values. This is important in the operation of the relaxation oscillator design.

PTM פורסם ב: