Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
mTouch-Slide27

Therefore, on the next TMR0 interrupt when the contents of the TMR1 registers are read, a smaller value than the previous interrupt should be retrieved. Comparing both values can identify a sensor touch. The frequency difference is exaggerated in the illustration to highlight these changes. In reality, a frequency change of between 1% and 5% can be expected.

PTM פורסם ב: