Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 24
The user can press the ‘Up’ and ‘Down’ buttons to select a specific file or folder. If the ‘Accept’ button is pressed when a folder is selected, the MicroSD Bootloader will display on the OLED the content of that specific folder. To return one level up, the user can either press the ‘Cancel’ button, or can use the ‘Accept’ button when the ‘..’ folder is selected. If the ‘Accept’ button is pressed when a HEX file is selected, the MicroSD Bootloader will prompt the user for a confirmation to load the file from the MicroSD memory card and to program it to the microcontroller’s Flash memory. After this operation is finished, the user may choose to execute that application or to remain in the bootloader. If the ‘Cancel’ button is pressed in the root directory, the MicroSD Bootloader will exit, and the last programmed application will be executed.
PTM פורסם ב: