Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 26
In this demo, the board will act like a USB mouse using the accelerometer as a tilt sensor. Hold the board flat relative to the ground for no movement.  If it is difficult finding the mouse cursor on the screen, please make sure that the board is flat relative to the ground.  Tilt the board to move the cursor.  Press the ‘L’ button to left click and the ‘R’ button to right click. Hold the menu button to return to the demo menu and to load a different application.
PTM פורסם ב: