Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 27
In this demo, the board will act like a USB joystick. Tilt the board to move the joystick on the X or Y axes; use the scroll bar to move it on the Z axes. Use the potentiometer to rotate around the Z axes, touch the ‘L’ and ‘R’ capacitive pads to control the first and second buttons. A test program is included in the application folder for the joystick demo that allows testing of the joystick features.  The “Game Controllers” option from the Microsoft Windows® “Control Panel” can also be used to show the joystick behavior. Hold the menu button to return to the demo menu and to load a different application.
PTM פורסם ב: