Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Product List
PIC18F MPLAB Starter Kit Slide 30
In this demo, the board will act like a USB Communication Device. When this demo application is connected for the first time to a host computer, it will ask for an INF file. In this case, point to the INF file provided on the CD-ROM disk in the CDC demo folder. After the complete enumeration, the board will appear like a serial port (COM) on the host computer and will start to send the raw data from the acceleration sensor. Use any form of HyperTerminal software and connect to the COM port created by the board to see the data. Hold the menu button to return to the demo menu and to load a different application.
PTM פורסם ב: