Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PAEC-Slide3

The ECAS series utilizes multilayer etched aluminum foil for anode and solid conductive polymer for negative cathode. The etched aluminum foil increases the surface area of the capacitor, thus increasing the capacitance value. The foil is oxidized to create the dielectric alumina (Al2O3). Alumina has very stable dielectric characteristics, making the capacitance of the ECAS series stable over temperature and voltage. Unlike MLCCs, polymer electrolytic capacitors have a marked polarity so proper placement on the PCB board is important. This also means that the ECAS series cannot be used in AC circuits.

PTM פורסם ב: