Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List
PAEC-Slide4

This slide provides a comparison of the conductivity of various electrolyte materials. The ESRs of the ECAS series are much lower than traditional aluminum and tantalum capacitors because conductive polymer has a conductivity which is 10,000 times higher than traditional electrolyte. Its conductivity is also higher than MnO2 or TCNQ complex salt which are often used for tantalum capacitors. Due to the multilayer structure and conductive polymer for negative cathode, this series achieves top-class low ESR compared with other types of electrolytic capacitors.

PTM פורסם ב: