Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LED Controllers Slide 12
The PCA967x family of devices are Fast-Mode Plus General Purpose I/O Expanders. In an application, the user may connect an LED from an I/O, via a current-limiting resistor, to VDD. By sending an I2C command to the device to drive the I/O low, the user may turn the LED light on. In the same token, by sending an I2C command to the device to drive the I/O high, the user may turn the LED light off. In this application, the GPIO may be used as an LED Switch. A drawback with this implementation is that every time the LED needs to be switched on or off, a command needs to be sent to the device. This can result in high bus traffic if the LED’s are switched on-and-off frequently.
PTM פורסם ב: