Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LED Controllers Slide 24
Comparing the two LED flash controllers from NXP, the SSL3250A is an asynchronous boost converter while the SSL3252 is a synchronous boost converter. The SSL3252 has the diode integrated in the device while the SSL3250A doesn’t and requires an external diode to be mounted on the PCB. The SSL3252 has built-in circuitry to detect a broken coil and hence fail safe, while the SSL3250A does not have the broken coil detection feature. The SSL3250A comes in a 16-terminal HVQFN package while the SSL3252 comes in a smaller 12-terminal chip scale package that is more suitable for handheld systems where space is a premium.
PTM פורסם ב: